text.skipToContent text.skipToNavigation

Legrand Expands Recall of Wiremold Under-Cabinet Power Strips Due to Electric Fire Hazard


WASHINGTON, D.C. - Consumers should stop using this product unless otherwise instructed. It is illegal to resell or attempt to resell a recalled consumer product.

 

Recall Summary


Name of Product:  Under-cabinet power strips

Hazard: The internal electrical connections of the power strips are substandard, posing risks of overheating and fire.

Remedy: Refund

Consumer Contact:  Legrand toll-free at (855) 692-4620 from 8 a.m. to 5 p.m. ET Monday through Friday, or at www.legrand.us and click on Recall Information for more information.

 

Recall Details


Units: About 46,000 in the U.S. and about 169 in Canada (About 14,200 were previously recalled September 2012)  

Description: This recall involves all Wiremold and Plugmold under-cabinet power and lighting strips with part number PX1001. The recalled power strips have four outlets and one fluorescent light and were manufactured from January 2011 through December 2013. From January 2011 through June 2012, the power strip came in a red package with the words “Legrand” and “Under Cabinet Power and Lighting” on the top front and “Wiremold-Series Part PX1001” on the bottom front. From July 2012 to April 2013, the power strip came in a white package with the word “Legrand” on the top front and “Plugmold Power Light,” “Under-Cabinet Power and Lighting” and “PX1001” on the bottom front. The manufacture date code is on the bottom of the recalled power strip in a circle with the year shown as "11," "12" or “13” in the center and an arrow pointing to the number representing the month. Part number PX1001, and UPC number 0 86698 00125 3, are imprinted on the bottom of the power strip.

Incidents/Injuries: The firm received one report of an incident. No injuries were reported

Remedy: Consumers should immediately unplug and stop using the power strips and return them to Legrand for a full refund.

Sold at: Ace Hardware, CED, City Electric, Cortland Wholesale, Crawford Electric, Do it Best, Hill Country Electric, Home Depot, Orgill, REXEL, Springfield Electric, Sutherland, TEC Electric, True Value Hardware and World Electric stores nationwide, and online at Amazon.com from February 2011 to April 2014 for about $40.

Importer: Legrand, West Hartford, Conn.

Manufactured in: China. 

Note: Health Canada's press release is available at http://healthycanadians.gc.ca/recall-alert-rappel-avis/hc-sc/2014/39511r-eng.php.

The U.S. Consumer Product Safety Commission is charged with protecting the public from unreasonable risks of injury or death associated with the use of thousands of types of consumer products under the agency’s jurisdiction.  Deaths, injuries, and property damage from consumer product incidents cost the nation more than $1 trillion annually. CPSC is committed to protecting consumers and families from products that pose a fire, electrical, chemical or mechanical hazard. CPSC’s work to ensure the safety of consumer products - such as toys, cribs, power tools, cigarette lighters and household chemicals – contributed to a decline in the rate of deaths and injuries associated with consumer products over the past 40 years.

Federal law bars any person from selling products subject to a publicly-announced voluntary recall by a manufacturer or a mandatory recall ordered by the Commission.

To report a dangerous product or a product-related injury go online to www.SaferProducts.gov or call CPSC’s Hotline at (800) 638-2772 or teletypewriter at (301) 595-7054 for the hearing impaired. Consumers can obtain news release and recall information at www.cpsc.gov, on Twitter @USCPSC or by subscribing to CPSC’s free e-mail newsletters. 

 

Right Rail:


CPSC Consumer Information Hotline

Contact us at this toll-free number if you have questions about a recall:
800-638-2772 (TTY 301-595-7054)
Times: 8 a.m. – 5:30 p.m. ET; Messages can be left anytime
Call to get product safety and other agency information and to report unsafe products.


Media Contact

Please use the phone numbers below for all media requests.
Phone: (301) 504-7908
Spanish: (301) 504-7800
Link Text: View CPSC contacts for specific areas of expertise

 
Stay Connected
CPSC Social Media icons


Report an Unsafe Product
We are still interested in receiving incident or injury reports that are either directly related to this product recall or involve a different hazard with the same product. 

In the future, CPSC plans to add automated safety tips and safety resource boxes to all recalls based on the high-level product category that this product falls in. Examples of high-level product categories are Toys, Baby Products, Sports Equipment, etc.